Plain bearing bushings & flanged bushings

Plain bearings with and without flange

The importance of plain bushings in mechanical engineering

one plain bearing and one rolling bearing, both made of metallic materials

Differentiation from rolling bearings

Typical areas of application for plain bushings


Types of plain bearing bushings

Plain bearing without flange, schematic drawing

Sleeve bearings (without flange)

Flanged bearing, schematic drawing

Bearings with flange

More types at a glance

Series / TypeIntended useGo to the online shop
Thrust washers Installation from the outside of the housing, easy replacementThrust washers in the online shop
Guide ringsPurely axial load, as a supplement to bushings, simple installation Guide rings in the online shop
Clip bearingsTool-free, simple installation; secure in sheet metal due to double flange Clip bearing in the online shop
Two hole flange bearingsViewable solution; can be used without toleranced housing bore Two hole flange bearings in the online shop
Double flange bearingSimple installation, secure in sheet metal due to double flange Double flange bearings in the online shop
Disc springsCompensation of axial play and manufacturing tolerances, damping effect Disc springs in the online shop
Split bearingsSimple retrofitting without dismantling the shaft Split bearings in the online shop
Pre-loaded two hole flange bearingsViewable solution; can be used without toleranced housing bore; clearance-free Preloaded two hole flange bearings in the online shop
Split bearings with anti-rotation featureSimple installation, compensation of tolerances, torsion-resistant Split bearings with anti-rotation feature in the online shop
Clearance-free preloaded flanged bearingsClearance-free and very quiet Clearance-free preloaded flanged bearings in the online shop

Materials for bearing bushings –

plastic vs. metal

various material granulates in horizontal test tubes

iglidur high-performance plastics

Tech up triangle

Benefits

Cost down triangle

Disadvantages

Sintered bronze

Tech up triangle

Benefits

Cost down triangle

Disadvantages

Sintered bronze metal with PTFE or POM gliding layer

Tech up triangle

Benefits

Cost down triangle

Disadvantages


iglidur plain bearings under scrutiny

iglidur plain bearing materials

The bestsellers: material recommendations

MaterialOptimised forTypical applicationMore material data
iglidur GAll-rounder – very low coefficients of friction, for edge loads & impactsAgricultural engineering, automotive, construction machinery, mechanical engineeringiglidur G material data
iglidur JPFPTFE-free, continuous use, low moisture absorptionVending machinery, printing industry, beverage industry, aviationiglidur JPF material data
iglidur A180High media resistance, food contactBeverage industry, food industry, medical technologyiglidur A180 material data
iglidur XHigh temperatures up to +250°C, contact with chemicalsFood industry, wood processing, plasticiglidur X material data
iglidur TX1Particularly economical, everyday applicationsConstruction machinery, agricultural engineering, heavy machinery, plant engineeringiglidur TX1 material data

From selection to installation

Various plain bearing types

Selecting the right plain bearing bushing

Plain bearing service life

Material selection and service life calculation

Installation of plastic bearings

Installation and tolerances

Consulting

I look forward to answering your questions

Treotham Automation Pty Ltd. (Distributor)(64) 7849 0281Write e-mail

Shipping and consultation