To prepare students optimally for their professional lives, universities try to convey their teaching content not only theoretically, but also practically. The case of the Technical University (TH) of Cologne showed that this is not always that easy. In the university's Mechanical Engineering Master's degree programme, production processes should not only be understood, but also experienced at first hand.
This is made possible by an Industry 4.0 demonstrator that maps a real production environment in miniature. Handling, material transport, and quality inspection in production are demonstrated on a compact table with a width of 900mm and a length of 1,200mm.
The challenge here: It was not just a question of finding an individual solution for the compact format of the conveyor line. A weight problem also had to be solved. Because the table had to be easy to push from one lecture hall to the next. A lightweight and compact solution had to be found for the cobot, which is intended to perform pick & place tasks on the conveyor belt, while at the same time fitting into the university's limited budget for didactic equipment. Because standard articulated arm robots on the market often cost tens of thousands of euros.