My contact person
e-chains®, chainflex®, cables, harnessed systems readychain®

(64) 9278 6577
dry-tech® bearing technology

(64) 9278 6577

Organ console

manus® 2007

The motion of the driving rod of an organ should be utmost noiseless and smooth-running. With it the organist is relieved on one hand, and on the other, undesired interfering sounds are avoided. At the same time a braking potential should be there. This was achieved by means of an adjusting screw.

The adjusting screw uses the elasticity of the applied iglidur® plastic bearing and marginally modifies the inner diameter. Thus a continuous braking action can be attained.

Csibi Ervin, Orgelbau Eisenbarth,
Passau

 
More on applied products here
Further interesting applications from extremely diverse areas can be found here.
Go to manus® contest