My contact person
e-chains®, chainflex®, cables, harnessed systems readychain®

(64) 9278 6577
dry-tech® bearing technology

(64) 9278 6577

Search for application examples

Improve technology and reduce costs

For years the igus® motto has been "plastics for longer life®". By this we mean the production of innovative plastic products which reduce maintenance work, achieve technical improvements, at the same time as reducing costs and increasing service life, everything delivered immediately from stock.

Our customers were able to improve the technology and reduce costs in more than 590 applications.
Some examples:

Longest travel in the world - no more downtimes

The longest travel with plastic energy chain  

The e-chain systems® today clearly contribute toward reliability, as system downtimes, for example through cable breaks, are reduced to zero.

Cables defy heat, sun, rain and snow

LED screen  

Previously used cables from a competitor had failed; since then the temperature-resistant chainflex® cables are used; the larger-than-life size LED screen in Dallas functions in any weather.

Rough environment, high speed

Special machine construction  

Even in particularly aggressive ambient conditions like in this high speed machining center, energy supply systems prove their reliability.

Costs saved, machine
availability increased

Beverages industry  

As iglidur® plain bearings have a long service life, and in addition need not be lubricated and costs only a fraction compared to conventional bearings, 90% of the costs could be saved.

More than Euro 10,000 saved each year

Fully automatic tire fitting lines  

The previously used bearings were blocked and the shafts used to break. The lubricant-free igubal® flange bearings used instead have been operating since May 2007 without failure. This saved Euro 2,440 in repair costs and Euro 8,400 in machine stoppages each year.

Trouble-free operation instead of shaft destruction

Concrete pipe cutter  

Due to the dirt accumulation in the ball bearings, the balls were blocked and the shafts were destroyed. The concrete cutting machine has now run for over three years entirely free of troubles despite the extremely heavy-duty operation.

Search

Are you looking for practically tested application examples in a certain industry?
Here you can browse through already implemented applications and filter them according to your specifications.

Industry sector:
Case of application:


Harbor crane

Circular motion mounted on the side in a harbor crane.

Harbor crane    

Stronger in the circle

Until recently, you could not purchase a solution anywhere in the world for this application.

Stronger in the circle    

Laser measuring telescope

The rotary motion in both directions by up to 310° is also possible at high speeds of up to 20 meters per second.

Laser measuring telescope    

Pallet changer

In the case of this application, the worksafety was increased by integrating theenergy supply system into the body of thepallet changer.

Pallet changer    

Screen facade for primary school

For wind and rain

Screen facade for primary school    

Camera jib

igus® goes to Hollywood - polymer plain bearings in a camera jib

Camera jib    

Suspended articulated arm robot

triflex® R as a complete solution for several tasks at once on a suspended robot

Suspended articulated arm robot    

Inlet control device

The plain bearings must withstand static radial loads of 25 N/mm² at temperatures of 170°C - 200°C.

Inlet control device    

Bank of lamps

This pivoted bank of lamps is equipped with 32 lamps à 4,000 Watts.

Bank of lamps    

Bucket wheel stacker

This contribution also concerns a circular application that has been designed with an igus® energy chain with rearward bending radius.

Bucket wheel stacker    

Test rig for solar systems

This test rig was able to be built thanks to the use of igus® e-chains®.

Test rig for solar systems    

Information board

This information board is exposed to the weather and the forces of nature all year round.

Information board    

Camera dolly 2

Another newly developed dolly for camera movement is the subject of this manus® contribution.

Camera dolly 2    

Hall crane equipment

This energy supply saves space by avoiding the trough.

Hall crane equipment    

Optical measuring device

Precise motions within the smallest spaces without electro-magnetic interference.

Optical measuring device    

Astronomical telescope

This telescope can be rotated from its original position in both directions by 270° each.

Astronomical telescope    

Truck washing bay

This washing system is installed under the open sky in Brazil.

Truck washing bay    

Scan system

This 3D scanning system allows simultaneous picture collection.

Scan system    

Sun protection system

This application shows an automated sun protection system with vertical lamellas.

Sun protection system    

Quad

The function of this gas handle for a quad or ATV can be executed via thumb gas or twist control handle.

Quad    

Shore power connections

At the Mongstad offshore base, flexible harnessed energy supply systems enable 3,000 shore-power connections per year.

Shore power connections    
Applications overview

I have the following project - following question - following request

No application example has been found here for your special case of application. Would you like to have further assistance?
Please let us know how we can help you!



Your data

Please always complete the fields marked *.

Company:*
First name:*
Last name:*
Phone:
Email:*
We need your post code and country so that we can forward your requests to the right contact person
Postcode:*
Country:*
If you would like to request catalogs or samples then please complete your address here.
Form of address:
Street:
Town:
State:
Yes, I would like to receive information on current products and services of igus® by e-mail. I agree to the exclusive use of my data by igus® in the framework of advertising messages in accordance with the data protection regulations. I am aware that I can withdraw my consent prospectively at any time by means of the "Unsubscribe" link contained in every e-mail.
I agree to the data protection regulations and the processing of my data. You can revoke this authorisation at any time.
Send